For complete ordering information, refer to the Metasys System Software Purchase Options Product Bulletin (LIT-12011703).
Product code | Product descriptions |
---|---|
M4-OASMIN-0 | License enabling OAS minimum software for a new site. |
M4-OASMIN-6 | License enabling OAS minimum software for upgrading existing site. |
M4-OASMIN-SCS | One-year site subscription service for OAS minimum software. |
M4-OASMIN-SC3 | Three-year site subscription service for OAS minimum software. |
M4-OASSTD-0 | License enabling OAS software. |
M4-OASSTD-6 | Upgrade for license enabling OAS software. |
M4-OASSTD-8 | License enabling OAS software for migrating OASMIN to OASSTD. |
M4-OASSTD-SCS | 1-year subscription for OAS software. |
M4-OASSTD-SC3 | 3-year subscription for OAS software. |
M4-OASPPA-0 | License enabling the Potential Problem Areas widget. |
M4-OASSCHRPT-0 | License enabling the Scheduled Reports feature. |
M4-OASHIST-0 | License enabling the Historical Data feature. |
M4-APIMOCMD-0 | License enabling the Monitoring and Commanding API. |
MS-SMP-6 | License enabling SMP for existing sites. Note:
This
is a one-time purchase license only available to customers
upgrading Metasys from a release before 12.0. Existing
customers who purchased MS-SMP-6 at Release 12.0 or later
can continue to use that same license after upgrading to
Release 14.0.
|
M4-BACNETSC-0 | License enabling BACnet Secure Connect |
Product code | Product descriptions |
---|---|
M4-OASTK-1 | Unlicensed OAS software and hardware turnkey solution. |
Code number | Description |
---|---|
M4-FAULT-0 |
License enabling Fault Detection feature for one Metasys server (ADS, ADS-Lite, ADX, or OAS series). 1 |
M4-TRIAGE-0 |
License enabling Fault Triage feature for one
Metasys server (ADS, ADS-Lite, ADX, or OAS series). 1
Note: M4-FAULT-0 is also required as a
prerequisite.
|
M4-FIPS-0 |
License enabling Federal Information Processing Standard 140-2 (FIPS 140-2 Level 1 compliance) for one Metasys server (ADS, ADS-Lite, ADX, or OAS series), or for one software network engine (NAE85 or LCS85 series). |
Field Ordering Instructions: When you process the order for the M4-OASTK-1, include the desired computer name in the order details. Email jciorder@jci.com with your order information, and request the computer name be added to the details of the M4-OASTK-1 line item. The repair center configures the computer name before loading the Metasys software.
For more information about changing the computer name, see the Appendix: Changing the OAS name and the computer name section in the Open Application Server (OAS) Commissioning Guide (LIT-12013243)