The M4-OASTK-1 OAS turnkey comes configured with all prerequisite and Johnson Controls software installed, has many recommended performance settings enabled, and has been tested and verified for proper functionality prior to shipment.
Figure 1. M4-OASTK-1
The M4-OASTK-1, built with 13th Gen Intel Core processors, Intel® Xe Graphics, and fanless chassis, delivers performance and innovation for use in small spaces, and embedded solutions without the use of a blower or fan.
Note:
The turnkey solution does not
support Fault Detection and Fault Triage.