Licensing - Metasys - LIT-12013309 - M4-APIMOCMD-0 - M4‑OASHIST-0 - M4‑OASMIN-0 - M4‑OASMIN-6 - M4‑OASMIN-SC3 - M4‑OASMIN-SCS - M4‑OASPPA-0 - M4‑OASSCHRPT-0 - M4-OASSTD-0 - M4-OASSTD-6 - M4-OASSTD-8 - M4‑OASSTD-SC3 - M4‑OASSTD-SCS - M4-OASTK-1 - Software Application - Open Application Server - 14.0

Open Application Server (OAS) Product Bulletin

Product name
Open Application Server
Document type
Product Bulletin
Document number
LIT-12013309
Version
14.0
Revision date
2024-07-30
Product status
Active

OAS requires a software license for its base product. Two licensing options are available for the OAS, the OAS minimum and the OAS standard. For more information about OAS licensing, refer to the Licensing section of the Open Application Server (OAS) Installation and Upgrade Guide (LIT-12013222)

If you install the OAS on a Windows Server operating system with SQL Server Standard or Enterprise, you need to purchase a Microsoft license. For more information refer to the Appendix: Microsoft Windows operating system and SQL Server software license requirements section in the Network and IT Guidance Technical Bulletin (LIT-12011279).
Note: Do not install the System Configuration Tool (SCT) or Controller Configuration Tool (CCT) on the OAS Turnkey computer. You must install the SCT and CCT on a different computer. If you host the OAS on a virtual machine (VM), you can install the SCT and CCT on the same VM as the OAS software.