Related documentation - Metasys - LIT-12013222 - M4-OASHIST-0 - M4-OASMIN-0 - M4-OASMIN-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASPPA-0 - M4-OASSCHRPT-0 - M4-OASSTD-0 - M4-OASSTD-6 - M4-OASSTD-SC3 - M4-OASSTD-SCS - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active
For information about Refer to
Commissioning the OAS Open Application Server Commissioning Guide (LIT-12013243)
Network and IT considerations Network and IT Guidance Technical Bulletin (LIT-12011279)
Metasys UI Metasys UI Technical Bulletin (LIT-12012115)
Metasys system features and benefits Metasys System Product Bulletin (LIT-1201528)
Metasys system general configuration Metasys System Configuration Guide (LIT-12011832)
Site Management Portal Metasys SMP Help (LIT-1201793)
How to license the OAS Software Manager Help (LIT-12012389)