Open Application Server introduction - Metasys - LIT-12013222 - M4-OASHIST-0 - M4-OASMIN-0 - M4-OASMIN-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASPPA-0 - M4-OASSCHRPT-0 - M4-OASSTD-0 - M4-OASSTD-6 - M4-OASSTD-SC3 - M4-OASSTD-SCS - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active

Use the following information to prepare your computer and install Metasys Open Application Server (OAS) software. The Open Application Server (OAS) is a product of the Metasys system that combines Metasys server and engine capabilities in a single software offering, with optional, add-on features.

As a Site Director, the OAS supports up to two supervisory devices, 200 field devices and 20,000 objects, provides database software options for archiving licensed historical data using the Microsoft® SQL Server software database, and enables secure communication to a range of network engines, including the NAE, NIE, NCE, SNE and SNC series engines.

OAS is available from Metasys Release 10.1 onwards. You can purchase an OAS as a software-only solution, that can reside on a virtual machine, or as a combined hardware and software turnkey solution. OAS supports both Metasys UI and Site Management Portal (SMP).