Modbus - Metasys - LIT-12013222 - M4-OASSTD-0 - M4-OASSCHRPT-0 - M4-OASSTD-SC3 - M4-OASSTD-SCS - M4-OASHIST-0 - M4-OASPPA-0 - M4-OASMIN-0 - M4-OASSTD-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASMIN-6 - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active

Modbus is one of the most common communication protocols used in the industry. It is openly published and royalty-free, making it relatively easy to deploy for an industrial network. Modbus transmits raw bits, or words without placing many restrictions on vendors. Metasys Network engines support both Modbus RTU (RS-485, RS-232) and Modbus TCP/IP connectivity. The OAS uses the default network interface and supports Modbus TCP/IP only. For more information, refer to the Network Engine Commissioning for Modbus Vendor Integration Application Note (LIT-12013150).