M-Bus - Metasys - LIT-12013222 - M4-OASSTD-0 - M4-OASSCHRPT-0 - M4-OASSTD-SC3 - M4-OASSTD-SCS - M4-OASHIST-0 - M4-OASPPA-0 - M4-OASMIN-0 - M4-OASSTD-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASMIN-6 - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active

M-Bus (Meter Bus) is a European standard (EN 13757-3) that applies to heat and electric meters. These meters measure the heat absorbed or released by an energy-conveying liquid in a heat-exchange circuit. An M-Bus level converter is necessary for an M-Bus integration. The converter connects a network engine to an M-Bus network.