Integrations - Metasys - LIT-12013222 - M4-OASHIST-0 - M4-OASMIN-0 - M4-OASMIN-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASPPA-0 - M4-OASSCHRPT-0 - M4-OASSTD-0 - M4-OASSTD-6 - M4-OASSTD-SC3 - M4-OASSTD-SCS - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active

The OAS supports integration with the following devices and systems. For more information, refer to the Adding a third party integration section in the NAE85 Commissioning Guide (LIT-12011044).