Upgrading an existing OAS installation - Metasys - LIT-12013222 - M4-OASHIST-0 - M4-OASMIN-0 - M4-OASMIN-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASPPA-0 - M4-OASSCHRPT-0 - M4-OASSTD-0 - M4-OASSTD-6 - M4-OASSTD-SC3 - M4-OASSTD-SCS - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active
To ensure that child devices appear in the Site Director's navigation tree, complete the following procedure to upgrade the OAS:
  1. Using the System Configuration Tool (SCT), upload your site to the archive database.
  2. Backup your archive database.
  3. Obtain the OAS installation file. When you download the Metasys Open Application Server folder from the License Portal, the folder contains two files: an executable file and a data file. You must keep the data file with the executable file in the same product folder.
    Important: If you separate the files within the product folder, the installation fails.
  4. A User Account Control dialog box appears. Click Yes.
  5. The Metasys Open Application Server Setup window appears. Click Install.
  6. Click Upgrade. The progress screen appears.
  7. When the installation completes, click Finish. If prompted, click Restart Now.