Uninstalling OAS software - Metasys - LIT-12013222 - M4-OASSTD-0 - M4-OASSCHRPT-0 - M4-OASSTD-SC3 - M4-OASSTD-SCS - M4-OASHIST-0 - M4-OASPPA-0 - M4-OASMIN-0 - M4-OASSTD-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASMIN-6 - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active
Note: Ensure that the OAS software can communicate with the SQL Server databases during the uninstallation process.
  1. Open Windows Control Panel.
  2. Open Uninstall a Program/Programs and Features.
  3. Right-click Metasys Open Application Server and select Uninstall/Change. The Open Application Server Setup window appears.
  4. If you want to retain the database during installation, clear the Remove databases check box.
  5. Click Uninstall.
  6. Click Finish.