Configuring a Virtual Machine for Metasys Server - Metasys - LIT-12013222 - M4-OASHIST-0 - M4-OASMIN-0 - M4-OASMIN-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASPPA-0 - M4-OASSCHRPT-0 - M4-OASSTD-0 - M4-OASSTD-6 - M4-OASSTD-SC3 - M4-OASSTD-SCS - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Brand
Metasys
Product name
Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

If you are installing the Metasys Server software on a virtual machine (VM), verify the following before you start to install Metasys:

  • Ensure that the virtual machine is running in static memory mode, not dynamic. Otherwise, operational issues with SQL Server may occur.
  • If you are upgrading from a hardware server to a VM, configure the Metasys Server VM with the same amount of memory as the hardware server, or with at least 8 GB of memory.
  • Set the hard drive size to fixed, not dynamic.
  • If required, add processor power to the VM.
  • In Microsoft Hyper-V, verify that the Process compatibility option under Virtual Machine Settings > Processor > Compatibility is not selected (Figure 1). For some Intel CPUs, this box is selected by default.
Figure 1. Processor compatibility setting on Metasys Server