Verifying the server certificate chain - Metasys - LIT-12013222 - M4-OASSTD-0 - M4-OASSCHRPT-0 - M4-OASSTD-SC3 - M4-OASSTD-SCS - M4-OASHIST-0 - M4-OASPPA-0 - M4-OASMIN-0 - M4-OASSTD-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASMIN-6 - Server - Open Application Server - 12.0

Open Application Server (OAS) Installation Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Installation Guide
Document number
LIT-12013222
Version
12.0
Revision date
2022-05-20
Product status
Active

About this task

To verify a certificate chain for a Metasys server or SCT computer:

Procedure

  1. In Control Panel, select System and Security > Administrative Tools and double-click Internet Information Services (IIS) Manager. The IIS main screen appears.
  2. Highlight the name of the web server.
  3. Under the IIS section in the middle pane, double-click Server Certificates. The Server Certificates panel appears.
  4. On the Actions pane, click View. The Certificate screen appears.
  5. Click the Certification Path tab. The certificate chain appears.
  6. Click OK to close the certificate view.