Requesting a server certificate - Metasys - LIT-12013222 - M4-OASHIST-0 - M4-OASMIN-0 - M4-OASMIN-6 - M4-OASMIN-SC3 - M4-OASMIN-SCS - M4-OASPPA-0 - M4-OASSCHRPT-0 - M4-OASSTD-0 - M4-OASSTD-6 - M4-OASSTD-SC3 - M4-OASSTD-SCS - Server - Open Application Server - 12.0
Open Application Server (OAS) Installation Guide
- Product
- Building Automation Systems > Application Servers > Open Application Server
- Document type
- Installation Guide
- Document number
- LIT-12013222
- Version
- 12.0
- Revision date
- 2022-05-20
- Product status
- Active
Procedure
-
In Control Panel, select and double-click Internet Information Services (IIS)
Manager. The IIS main screen appears.
-
Under the IIS section in the middle pane, double-click Server
Certificates. The Server Certificates panel appears.
-
On the Actions pane, click Create Certificate Request. The Distinguished
Name Properties screen appears.
-
Fill out all the fields in the form. For Common name, specify
the full computer name, which you can determine from . The full name may also include a domain name (for example,
MAIN-ADX.mycorp.com). Click Next. The
Cryptographic Service Provider Properties screen appears.
-
Select an appropriate service provider and bit length. Click Next. The
File Name screen appears.
-
Click the Browse (...) button to select a location where to save the
certificate request file. The Specify Save as File Name window appears.
-
Type in a file name and click Open. The File Name window appears with
the file name specified.
-
Click Finish. The certificate request file with a .txt extension is
created in the selected folder. For example, the certificate request file for a
server called MAIN-ADX would be MAIN-ADX.txt.
-
Send the certificate request file to the IT department or CA to obtain your
trusted certificate. When you receive the file, go to Completing a server certificate request to import the
certificate into the server.