OAS and SCT temporary file cleanup - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

Computers with OAS and SCT software generate temporary and transient files related to the operation of the OAS and SCT. These files can accumulate and reduce the available hard disk space. You can delete or move these files offline to help save on hard disk space.

The Metasys system folders with temporary and transient files are either located in C:\Users\All Users\Johnson Controls\MetasysIII or C:\ProgramData\Johnson Controls\MetasysIII.

Note: Do not install the SCT on the OAS Turnkey computer, you must install the SCT on a different computer. If you host the OAS on a virtual machine, you can install the SCT on the same VM as the OAS software.

The particular subfolders that contain temporary or transient content are:

  • \Diagnostics
  • \download
  • \FileTransfer
  • \SecurityFiles
  • \temp
  • \upload

When you delete or move the files under these folders, do not delete or move the folders themselves, just the subfolders and any files under the subfolders. Also, do not disturb any other MetasysIII folders that are not listed here.