The Trend repository database resides on the OAS within the SQL Server software database.
The installation program places the Trend repository on the same computer where the OAS software resides. The default directory location is C:\Program Files\Microsoft SQL Server\MSSQL<version>.MSSQLSERVER\MSSQL\DATA.
If you want to change where the databases are loaded, you need to do so before you install OAS. For details, refer to the Open Application Server (OAS) Installation Instructions (LIT-12013222).
- configure larger sample intervals for individual trends
- determine which trends to store long-term and transfer only these samples
- configure the trends of non-critical objects to sample on large Change-of-Value (COV) increments
In addition, you can optimize the network communication performance for transferring trend samples from engines to the OAS repository by configuring the Transfer Setpoint on individual trends so they transfer their samples at intervals different from other trends.
Refer to the Trend Extensions topic in the Metasys SMP Help (LIT-1201793) for more information.