Antivirus software - Metasys - LIT-12013243 - M4-OASMIN-0 - M4-OASSTD-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product name
Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

To maintain the integrity of your system, run frequent virus scans of the computer running the Server. Use one of the following antivirus software programs:

  • Symantec® Endpoint Protection software Corporate Edition Version 12.x or higher.

  • McAfee® VirusScan® Enterprise version 8.8 with Patch 9 or later.

  • Windows Defender® built into Windows 11®, Windows 10®, Windows Server 2019®, Windows Server 2022® .

For more information, refer to the Appendix: Installing antivirus software section in the Open Application Server (OAS) Commissioning Guide (LIT-12013243).