Summary of changes - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active
The following information is new or revised:
  • Updated OAS technical specifications.
  • Added support for Microsoft Windows® 11.
  • Added support for Microsoft Windows Server® 2022.
  • Added support for SQL Server® 2022.
  • Removed support for SQL Server® 2016.
  • Removed support for Microsoft Windows Server® 2016.