Open Application Server introduction - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

The Open Application Server (OAS) software contains features and configurations that are not set up by the default installation or license selection. This document describes the workflow for how to commission the OAS as part of a Metasys system, and set up and modify the configuration of the OAS to better suit the needs of your facility.

For OAS hardware and software requirements, refer to the Open Application Server (OAS) Installation Guide (LIT-12013222) and the Metasys System Configuration Guide (LIT-12011832).