The OAS Turnkey has the following specifications:
| Processor | Intel® Core i5-1340P |
| Operating system |
Windows 11 IoT Enterprise |
| Database software | SQL Server 2019 Express with CU18 (64-bit) |
| Memory | 32 GB DDR4-3200 SODIMM |
| Power input | 19V DC rear jack. 12-20v operation. 19VDC65W power supply included |
| Storage | 256 GB SSD |
| Networking |
Intel Wi-Fi 6E AX211 2.5Gb LAN (i226V) |
| Input/Output |
Two Thunderbolt 4 Three USB 3.2 Type-A One USB 2.0 Type-A |
The following table is for software-only OAS servers. If you install the OAS on a virtual machine, review Table 2 to verify that you meet the minimum hardware and software requirements.
| Recommended computer platform |
Intel Core i7-8700 Processor, Six Cores, 3.20 GHz or better Note: Match the specs of the ADS/ADX recommendations that
correspond to the site characteristics. For example, the number of
users, the number of engines and objects, and site traffic. If you
host the OAS on a virtual machine, match the recommendations listed
in the Network and IT Guidance Technical
Bulletin (LIT-12011279).
Two 500 GB hard disks with 40 GB free space after you install all prerequisite software and before you install OAS software. Configure RAID 1 (mirroring) with disk write caching enabled. Note: Prerequisite software includes the supported
operating system, database software, and .NET Framework.
|
| Memory |
Minimum: 32 GB |
| Supported desktop operating systems and database software |
Windows® 11 Pro and Windows® 11 Enterprise versions 22H2, 21H2 (64-bit) General Availability Channel (GAC) Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). Windows® 10 Enterprise LTSC (1809, 21H2) (64-bit)Supports:
|
| Supported server operating systems and database software |
Windows® Server® 2022 (64-bit) Windows® Server® 2019 (version 1809 or later) (64-bit) Supports:
|
| Supported user interfaces |
Metasys User Interface Site Management Portal (SMP) Note: SMP requires a license at
Release 13.0. The license
is available only to existing Metasys customers. If
you licensed SMP at Release 12.0, you can use the same license
after you upgrade to Release 13.0.
|
| Supported virtual environments |
Microsoft Hyper-V™ VMware® |
| Additional software included with the OAS software download |
Microsoft .NET Framework Version 4.7.2 Microsoft .NET 6.0.16 RabbitMQ Server 3.8.16 Erlang OTP 23.2 (11.1.4) Launcher Software
Note:
You can find the Launcher
resource files at the following website: http://www.johnsoncontrols.com/buildings/specialty-pages/metasys-launcher
|
| Optional software |
Metasys Database Manager Language Installation Program |