Setting power failure options for the OAS - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

About this task

Follow these steps to make sure your computer comes back online after a power failure. This procedure requires that you access the computer’s BIOS settings while the computer is starting up.

Accessing and changing BIOS settings may vary depending on the computer you are using. Seek input from the IT department if you are unsure how to change the computer’s BIOS settings.

Note: You may want to use an Uninterruptible Power Supply (UPS) to prevent your computer from going offline during a power failure.

Procedure

  1. Restart the computer. While the computer is starting up, press the appropriate key to enter Setup mode (for example, F10).
  2. Edit the appropriate Power Management settings so the computer restarts after a power failure (for example, set After Power Failure to Switch On).
  3. Save changes and exit Setup mode.