Configuring an OAS as Site Director - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

The OAS installation process sets the OAS to be its own Site Director. So, by default, the OAS on a site is the Site Director. OAS does not support the configuration of multiple OAS or any other server, nor the addition of any type of server as a child under OAS.