Creating audit entries for discard events - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

About this task

By default, the OAS does not create an audit entry when you discard an event that originates on the OAS .

Procedure

  1. On the OAS computer, right click Notepad and select Run as administrator.
  2. Using Notepad, open the following file:

    C:\Program Files (x86)\Johnson Controls\MetasysIII\WS\web.config

  3. Find the line for WriteAuditAckDiscard:

    add key="EventRepository.WriteAuditAckDiscard" value="false"/

  4. Change the value from false to true.
  5. Save the file and close all windows.
  6. Restart the OAS