Changing the action queue timeout - Metasys - LIT-12013243 - M4-OASMIN-0 - M4-OASSTD-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

You may need to change this setting if you download a large number of user views or graphics that reside on a subnet different from the SCT. In this situation, the Action Queue may time out before the download is complete. The default value for the Action Queue timeout is 30 seconds.

This setting is handled in the SCT. Refer to Metasys SCT Help (LIT-12011964) for details on changing this setting.