Configuring Metasys system settings - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

The Metasys system administrator can modify default settings manually, if needed.

The settings in this section reset to their default values when you upgrade the system. Reconfigure the settings as required.