BACnet time synchronization - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

BACnet time synchronization uses BACnet protocol to synchronize with BACnet devices such as the network engine. Use this method when the Site Director has access to a BACnet time server. This method is not available on the Metasys server.