Verifying the Site Director defined for an engine/server - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

About this task

For time synchronization to work properly, all engines/servers on a site must have the correct name for the Site Director in the Local Site Director attribute. If an engine/server has the incorrect device defined as Site Director, time synchronization may not work properly on your Metasys site.

Procedure

  1. Log in to the engine/server.
  2. Drag and drop the engine/server object to the Display frame.
  3. Select Advanced.
  4. Scroll to the Site section and verify that the Local Site Director attribute contains the correct device
    Notes:
    • The Local Site Director may be entered as an IP address or host name. If entered as a host name, the name is case-sensitive (for example, NxE-THREE is not the same as nxe-three ).
    • If the Site Director field contains the incorrect device or is empty, click Edit. Edit the Site Director entry and click Save.
  5. Go to Setting the time synchronization method.