Setting the time zone in the Site Director OAS - Metasys - LIT-12013243 - M4-OASMIN-0 - M4-OASSTD-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

Procedure

  1. In the lower-right corner of the OAS computer screen, click the time. The Date and Time Properties box appears (Figure 1). The appearance of this screen varies depending on the operating system.
    Figure 1. Time and Date on a Site Director

  2. Click Change date and time settings, then click Change time zone. The Time Zone Settings box appears.
  3. Select a time zone from the drop-down list box.
  4. Select Automatically adjust clock for Daylight Saving Time, if present.