Setting the date and time in the Site Director OAS - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

About this task

Before manually setting the date and time in the Site Director OAS , follow the steps in the Setting the time zone in the Site Director OAS section.

Procedure

  1. Click the time in the lower-right corner of the screen. Click Change date and time settings.
  2. Set the time and date.
  3. Click OK.

    The Site Director time zone, date, and time are now set and propagate to all other engines/servers on the site.