Steps for successful time management - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

About this task

For successful time management, do the following:

Procedure

  1. Verify that each non-supervisory engine/server on the Metasys network has the correct Site Director defined.
  2. Set the time synchronization method for the site.
  3. Set the default time zone of the Site object for each network engine that has Metasys software at Release 8.0 or later.
  4. Set the time zone and then set the date and time or select a site time server for the site.

    See the OAS as Site Director section.

    If you have an OAS as the Site Director, the time zone, date, and time are set in the Windows operating system of the computer where the OAS resides. See the OAS as Site Director section.

  5. For Multicast time synchronization only, configure the SNTP Multicast attributes for the site.