OS licensing modes and CAL examples - Metasys - LIT-12013243 - M4-OASMIN-0 - M4-OASSTD-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

Figure 1 illustrates the use of CALs in a Metasys network.

Figure 1. Example Network in Per Device or Per User Operating System Licensing Mode