Restoring default system preferences - Metasys - LIT-12013243 - M4-OASMIN-0 - M4-OASSTD-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

Procedure

  1. Access the Metasys system device on which you want to restore the default system preferences.
  2. Navigate to the Preferences directory for the device as shown in Table 1.
  3. Delete the SystemPreferences.xml file.