Removing user preference files - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

Procedure

  1. Access the Metasys device from which you want to remove the user preference files and navigate to the Preferences directory for the device as shown in Table 1.
  2. Delete files named UserPreferences-userID.xml, where userID is the identification number that appears in the Security Administration tool.
    Note: Do not delete DefaultUserPreferences.xml.