Uploading the Metasys archive database - Metasys - LIT-12013243 - M4-OASMIN-0 - M4-OASSTD-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active
  1. Launch SCT, log on, and then open the relevant archive.
  2. In the Metasys Rename Assistant, click Next, and then, in the SCT, select the Metasys server in the navigation tree.
  3. In the Metasys Rename Assistant, click Next, and then, in the SCT, from the Tools menu, select Manage Archive.
  4. In the Manage Archive wizard, click Next.
  5. On the Action page, select Upload from Device, and then click Next.
  6. In the Metasys Rename Assistant, click Next.
  7. In the Manage Archive wizard, on the Select Devices page, select the Metasys server in the navigation tree, and then click Next.
  8. In the Metasys Rename Assistant, click Next, and then, in the Manage Archive wizard, on the Schedule page, click Next.
  9. In the Metasys Rename Assistant, click Next, and then, in the Manage Archive wizard, on the Site Login page, click Test Login, and then click Next.
  10. In the Metasys Rename Assistant, click Next, and then, in the Manage Archive wizard, on the Repeat Upload page, click Next.
  11. In the Metasys Rename Assistant, click Next, and then, in the Manage Archive wizard, on the Summary page, click Finish.
    Note: After the upload completes, the site and server names now match.
  12. In the Metasys Rename Assistant, click Next, and then exit the SCT.
  13. Click Continue.
    Note: If you are not using the Metasys Advanced Reporting System, the verification and rename processes are complete.