Reinstalling the Metasys software - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document type
Commissioning Guide
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active
  1. Click MDM Rename.
    1. In the Metasys Database Manager, click the Rename tab.
    2. In the Old field, enter the old Site Director name. This is found in red text in the pop-up instructions with the Metasys Rename tool.
    3. In the New field enter the old Site Director name, this is found in red text in the pop-up instructions with the Metasys Rename tool.
      Note: Ensure you use the proper name format. Enter the Old value in the format SiteDirector:SiteDirector or SiteDirector:Device. Enter the New value in the format NewSiteDirector:NewSiteDirector or SiteDirector:Device.
    4. Click Rename Now.
    5. Close the Metasys Database Manager.
  2. Click Browse under Install Metasys SCT. Browse to the SCT installation file, and then click Open.
  3. Click Install.
    1. In the SCT installation window, click Install.
    2. Select the server from the Server Name list, and then click Install.
    3. Click Finish.
  4. Click Browse under Install Metasys OAS , browse to the Metasys server installation file, and then click Open.
  5. Click Install.
    1. In the Metasys Server installer, click Install.
    2. Select the server from the Server Name list, and then click Install.
    3. Click Restart Now.