Appendix: Changing the OAS name and the computer name - Metasys - LIT-12013243 - M4-OASSTD-0 - M4-OASMIN-0 - Server - Open Application Server - 13.0

Open Application Server (OAS) Commissioning Guide

Product
Building Automation Systems > Application Servers > Open Application Server
Document number
LIT-12013243
Version
13.0
Revision date
2024-06-12
Product status
Active

Follow the steps in this section to change the name of an OAS. The name and the computer name must match for proper functionality.

Important: After you follow these procedures for a Site Director, the fully qualified item references have the new name and do not match the fully qualified item references in historical data. For tools that access historical data, such as the Metasys Export Utility, you may need to use the old item references to retrieve data.