Summary of changes - Metasys - LIT-1201990 - Software Application - NxE Information and Configuration Tool - 10.1

NxE Information and Configuration Tool Technical Bulletin

Product
Building Automation Systems > Configuration and Programming Tools > NxE Information and Configuration Tool
Document number
LIT-1201990
Document revision
Version
10.1
Revision date
2019-10-14

The following information is new or revised:

  • Updated screens throughout the document to indicate the new or revised content.
  • Added two new models of network engines that the NCT supports: SNE (network engine with no equipment inputs/outputs) and SNC (network engine with equipment inputs/outputs).
  • Replaced the term NxE with network engine throughout document to include the naming of the new models, the SNE and SNC.
  • Added content that mentions FTP operations are not available on newer network engines with the Microsoft® Windows® Embedded operating system unless the firewall is disabled manually.