About this task
Use these procedures to transfer files between your NCT computer and NAE35, NAE45, and NCE25 engines. FTP also works with the NAE55-1 and NAE55-2. FTP operations are available only to network engines that are running a Windows Embedded OS whose firewall is disabled. For network engines with Linux, refer to Using SSH connection in the Advanced mode.
Note: The NCT enables you to start/set up an
FTP or Telnet session with a connected NAE35, NAE45, or NCE25 engine using the
Connect FTP and Connect Telnet buttons on the Connections tab when the NCT is in Advanced mode. See Tools tab for more
information. We recommend starting an FTP or Telnet session from the Connections tab.
To set up FTP and Telnet servers on the Connection tab: