About this task
To enable the Advanced mode on the NCT:
Procedure
- On the Start menu, go to Programs > Johnson Controls > Metasys and hover over NAE Information and Configuration Tool to highlight the option.
-
With the NAE Information and Configuration Tool option highlighted, right-click
and select Properties. The NAE Information and
Configuration Tool Properties dialog box appears (Figure 1).
Figure 1. NCT Properties dialog box
- Select the Shortcut tab and enter a space followed by /advanced at the end of the string in the Target field (Figure 1).
-
Click OK. The properties are updated and
Properties box closes.
The next time you start the NCT, it runs in the Advanced mode.