Using the Advanced mode - Metasys - LIT-1201990 - Software Application - NxE Information and Configuration Tool - 10.1

NxE Information and Configuration Tool Technical Bulletin

Product
Building Automation Systems > Configuration and Programming Tools > NxE Information and Configuration Tool
Document type
Technical Bulletin
Document number
LIT-1201990
Document revision
Version
10.1
Revision date
2019-10-14

The Advanced mode of NCT enables extra features not available under Normal mode. For network engines using a Windows Embedded OS, an FTP server (NAE55-1, NAE55-2, NAE35, NAE45, and NCE25) or a Telnet server (NAE35, NAE45, and NCE25) is available. For network engines with a Linux OS, a secure shell connection (SSH) is provided.

The Advanced mode has some powerful options that allow you to update files on the device; however, users should avoid indiscriminate use of the Advanced mode features. Only use the Advanced mode as directed in Johnson Controls documentation or under the direction of your local Johnson Controls service/support representative.

For information on enabling Advanced mode, see Enabling Advanced mode.