The NCT allows users to copy files from their local machine to network engines that are running a Windows Embedded OS. For information about copying files or transferring files, see Using FTP and Telnet servers in the Advanced mode and FTP sessions between NCT and network engines. For information about copying files or transferring files for network engines with the Linux OS, see Using SSH connection in the Advanced mode and Finding and sending non-crash files on a network engine.