Monitoring Engine Messages - Metasys - LIT-1201990 - Software Application - NxE Information and Configuration Tool - 10.1

NxE Information and Configuration Tool Technical Bulletin

Product
Building Automation Systems > Configuration and Programming Tools > NxE Information and Configuration Tool
Document number
LIT-1201990
Document revision
Version
10.1
Revision date
2019-10-14

The NCT allows users to monitor engine messages on the Connections tab. These messages relay high-level events, and they can be helpful when installing patches.

To view engine messages, look in the Messages From Selected Devices pane (Figure 2).

To clear messages, click Clear Messages.

Note: If you are using messages for troubleshooting, use the NAE Update Tool to monitor engine messages. For more information on this tool, refer to NAE Update Tool Help (LIT-12011524) .