The following table provides the minimum computer and OS software requirements for installing the NCT on a laptop, computer, or server. These computer platform and memory recommendations are not meant to imply that older or slower machines are not usable. Refer to the Network and IT Guidance Technical Bulletin (LIT-12011279) for more information regarding computer/server recommendations.
Recommended Computer/Server Platform |
Intel Core 2 Duo E6700 or higher (Intel Core 2 Duo E4300 minimum) 20 GB free hard disk space available (600 MB minimum) DVD drive |
Recommended Memory |
Computer Platforms: 2 GB RAM (1 GB RAM minimum) Server Platforms: 4 GB RAM (2 GB RAM minimum) |
Supported Operating Systems |
|
Network Communication |
Ethernet network interface card 10/100/1,000 Mbps (a 100 or 1,000 Mbps network connection is recommended) |