Installation steps - Metasys - LIT-1201990 - Software Application - NxE Information and Configuration Tool - 10.1

NxE Information and Configuration Tool Technical Bulletin

Product
Building Automation Systems > Configuration and Programming Tools > NxE Information and Configuration Tool
Document type
Technical Bulletin
Document number
LIT-1201990
Document revision
Version
10.1
Revision date
2019-10-14

About this task

Note: The laptop, computer, or server on which you intend to install the NCT must meet the minimum requirements described in Minimum computer and operating system requirements. Also, you must remove any previous release of NCT before installing a new release of the NCT.

To install the NCT:

Procedure

  1. Navigate to the NAE Configuration Tool folder on the product disk and double-click the NICTool.exe file. The Welcome screen appears (Figure 1).
    Figure 1. NCT Installation Wizard start screen

  2. Click Install.
    Note: If the WinPcap utility is not already installed on your computer, a WinPcap Setup Wizard screen appears during NCT installation (Figure 2). If WinPcap is already installed on your computer, the WinPcap Setup Wizard does not appear. Go to Step 6 to complete installation the NCT.
  3. Click Next in the WinPcap Setup Wizard welcome screen (Figure 2) to start the WinPcap installation.
    Figure 2. WinPcap Setup screen

  4. Accept the default values and settings on all screens of the WinPcap Setup wizard.
    Figure 3. WinPCap Installation Wizard Finish screen

  5. Click Finish (Figure 3). The WinPcap Setup Wizard closes and NCT setup continues.
  6. Click Finish in the NCT InstallShield Wizard complete screen (Figure 4). The NCT is now installed and ready for use.
    Figure 4. NCT Installation Wizard Complete screen