Get all Debug files - Metasys - LIT-1201990 - Software Application - NxE Information and Configuration Tool - 10.1

NxE Information and Configuration Tool Technical Bulletin

Product
Building Automation Systems > Configuration and Programming Tools > NxE Information and Configuration Tool
Document number
LIT-1201990
Document revision
Version
10.1
Revision date
2019-10-14

The Get All Debug Files function allows you to retrieve and store the debug files that the NCT generates.

The NCT saves several types of debug files, including .log, .map, .txt, and others. Figure 2 shows an example of the Device Manager log file (dmlog.txt) file from a network engine with the Windows Embedded CE OS.

The debug files are saved in the same directory structure as they are stored on the network engine. The directory created by the Get All Debug Files process for an NAE35, NAE45, or NCE25 is shown in the square in Figure 2.

For more information on using this feature, see Finding crash files.