Trace feature - Metasys - LIT-1201990 - Software Application - NxE Information and Configuration Tool - 10.1

NxE Information and Configuration Tool Technical Bulletin

Product
Building Automation Systems > Configuration and Programming Tools > NxE Information and Configuration Tool
Document number
LIT-1201990
Document revision
Version
10.1
Revision date
2019-10-14

The trace feature in the Device Snapshot tool allows you to determine which:

  • threads are associated with which process

  • modules (DLL files) are associated with which process

  • window is held open by which process

Click any line in any pane and all of the connections are highlighted for you. As shown in Figure 1, the selection in the Processes pane causes the associated threads, modules, and windows to be highlighted in their respective panes.

Figure 1. Device Snapshot Trace Feature