Connect FTP on the Connections tab - Metasys - LIT-1201990 - Software Application - NxE Information and Configuration Tool - 10.1

NxE Information and Configuration Tool Technical Bulletin

Product
Building Automation Systems > Configuration and Programming Tools > NxE Information and Configuration Tool
Document number
LIT-1201990
Document revision
Version
10.1
Revision date
2019-10-14

When your NCT computer is connected to an NAE55-1, NAE55-2, NAE35, NAE45, or NCE25 and the NCT is running in Advanced mode, you can click Connect FTP on the Connections tab to automatically start an FTP session using Internet Explorer. The FTP session stops when you disconnect the NxE from the NCT. You can also stop the FTP session by clicking Stop FTP on the Tools tab.

Using the Connect FTP button on the Connections tab is the recommended method for setting up an FTP session. See Using FTP and Telnet servers in the Advanced mode for more information.