This section describes the NCT screens, tabs, features, functions, and the associated user actions for the NCT user interface.
Note: The NCT can operate in Normal mode or Advanced
mode. Typically, you should use the NCT in Normal mode. Use the Advanced mode with the
guidance of your local Johnson Controls® service/support
representative. The NCT screens in this document are shown in the Advanced mode to
display all available features. Items that appear only in Advanced Mode are highlighted
in gray. See Using the Advanced mode for more information.