The following table lists the latest Metasys system software releases of each network engine model along with the security attributes available for each. As the security features of the Metasys system have improved with each new software release, the network engines have likewise been improved.
|
Release with Security Attributes |
MS-NCE25xx-0, MS-NIE29xx-0, MS-NAE35xx-2, MS-NIE39xx-2, MS-NAE45xx-2, MS-NIE49xx-2 |
MS-NAE55xx-2, MS-NIE59xx-2 |
MS-NAE55xx-3, MS-NIE59xx-3 |
M4-SNCxxxx0-x, M4-SNCxxxx1-x, M4-SNCxxxx2-x |
M4-SNCxxxx1-xH, M4-SNCxxxx2-xH |
M4-SNExxxx0-x, M4-SNExxxx1-x, M4-SNExxxx2-x |
NAE85, NIE89 |
|---|---|---|---|---|---|---|---|
|
Release 9.0 to 9.0.6
|
X |
X |
X |
N/A |
N/A |
N/A |
X |
|
Release 9.0.7 or later
|
X |
N/A |
N/A |
N/A |
N/A |
N/A |
N/A |
|
Release 10.0
|
N/A |
X |
X |
N/A |
N/A |
N/A |
X |
|
Release 10.1
|
N/A |
X |
X |
X |
N/A |
X |
X |
|
Release 11.0
|
N/A |
X |
X |
X |
X |
X |
X |
|
Release 12.0
|
N/A |
N/A |
X |
X |
X |
X |
X |
|
Release 13.0
|
N/A | N/A | N/A | X | X | X | X |