Supported .NET Core Versions and Upgrades - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

From Release 10.1, Metasys installs include .NET Core components. The following table lists the Metasys system software releases and the associated .Net version along with the upgrade options available for each.

Table 1. Supported .NET Core Versions and Upgrades
Metasys Version .NET version Upgrade options
Metasys 10.0/10.1 .NET Core 2.1.5 N/A
Metasys 11.0.0/11.0.1/11.0.2 .NET Core 2.1.17 These can be updated to the latest minor version of .NET Core 2.1.x.
Metasys 11.0.3/12.0.0/12.0.1 .NET Core 3.1.17 These can be updated to the latest minor version of .NET Core 3.1.x.
Metasys 11.0.4/12.0.2/13.0 .NET 6.0.5 These can be updated to the latest minor version of .NET 6.0.x.