Metasys Advanced Reporting System UI - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active

The Metasys Advanced Reporting System offers a separate HTML-based user interface in which you can run reports on system configuration and performance. This system allows you to use a restricted access user interface and avoid Java software downloads for users with limited report and configuration needs.

The Metasys Advanced Reporting System can be used only on ADXs that are running a supported SQL Server software version with SQL Server Reporting Services. Local Metasys system users with Standard Access access type privileges are authorized with the Advanced Reporting option in the Security Administrator System.

For more information, refer to the Metasys Advanced Reporting System Help (LIT-12011312) .